DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
Image flip can be used to compensate for folds in the optical path. The default image flip settings are stored in flash and the values are specified in the flash header file. Image flip values may also be set using the Display Image Orientation command. This command is a "Hold Source" command which means that changes will not be applied until the source is changed. To do this, the Prepare for Source Change command should be sent followed by the Source Select command in order to apply the source changes. These steps are shown as follows:
Flip can be performed along two axes: a short axis flip and a long axis flip. Flips along both axes are shown in Figure 5-15 and Figure 5-16. Any combination of these two flip settings is permitted.