DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
This command is used to read status information from the diagnostic interface.
Command Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
2:1 | 15:0 | Start Index 0-based index of the first desired byte value to be returned. 0 - 63 LSByte = Byte 1 |
4:3 | 15:0 | Number of Bytes 1-based number of data bytes to be returned. 1 - 64 Start Index + Number of Bytes must be less than or equal to 64. LSByte = Byte 3 |
Return Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 ... n | Data Bytes Data values to return. The number of bytes is determined by the "Number of Bytes" field specified in the command parameters. |