DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
The 32-bit CRC is implemented as follows:
The bytes within each word (4 bytes) of data must be reversed prior to the CRC calculation. For example, using the data word 0xAABBCCDD, the value to be used in the CRC is 0xDDCCBBAA.
The CRC must include all words in the scratchpad block starting after the "Size" field and including all padding bytes up to the flash sector size.