DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
This command is used to specify an override temperature value to use for dimming compensation.
Write Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
2:1 | 15:8 | Temperature Integer Celsius Two's complement integer portion of temperature 127 = 127 Celsius 128 = –1 Celsius |
7:4 | Temperature Fraction Celsius 1/16 Celsius steps always added to the integer portion. Note that this fraction is still added even if the integer portion is negative. 1 = 0.0625 Celsius 2 = 0.125 Celsius | |
3:0 | Reserved |