DLPU048E August 2016 – July 2024
This command is used to verify the contents of the flash device.
The Request in Progress bit of the Short Status will be set at the start of the flash verify process and will be cleared when the verify process is complete. The error bits of the Short Status can be read to determine if an error occurred during the flash verify.
More information on flash programming can be found in Section 5.3.
Write Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 | 7:0 | Flash Data Type Refer to Table 8-86 for options. |
The flash data types are described in Table 8-86.
FLASH DATA TYPE VALUE | DESCRIPTION |
---|---|
0x00 | Entire flash |
0x01 | Entire flash except scratchpad data |
0x30 | Main Application |
0x40 | Configuration Data 0 |
0x50 | Configuration Data 1 |
0x60 | Batch command sets |
0x90 | Splash Data 0 |
0x91 | Splash Data 1 |
0x92 | Splash Data 2 |
0x93 | Splash Data 3 |
0x94 | Splash Data 4 |
0x95 | Splash Data 5 |
0x96 | Splash Data 6 |
0x97 | Splash Data 7 |
0xA0 | Scratchpad Data 0 |
0xA1 | Scratchpad Data 1 |
0xA2 | Scratchpad Data 2 |
0xA3 | Scratchpad Data 3 |