DLPU048E August 2016 – July 2024
When the ADC Single Measurement command is received by the DLPC230-Q1 main application, it will request an ADC capture from the TPS99000-Q1 for the specific ADC multiplexer index that is specified by the command, from 0 to 31. Note that this index is different than the DLPC230-Q1 memory index which is not relevant for a single ADC measurement.