DLPU048E August 2016 – July 2024
This implementation uses one pixel in a corner of the active video. The red and green values of this pixel are set to 0, and the blue value is incremented from 0 to 7 each frame. This pixel remains effectively black across all frames due to the low maximum pixel value (R 0, G 0, B 7). The value of the frame counter checksum is equal to the blue value of this single pixel since it is the only pixel within the checksum region and its red and green values are 0.