DLPU048E August 2016 – July 2024
HOST_SPI_MODE is configured as an output and toggled during DLPC230-Q1 software initialization to aid in debug. This begins immediately after the value is read as an input. Figure 2-2 shows the initialization events and the associated HOST_SPI_MODE signal. A toggle will occur for optional events regardless of whether they are enabled or disabled so that events following can still be properly identified.
The tests are described in Section 6.4.2. BIST 1 is the DLPC230-Q1 Command and Flash Interface Memory Test.