DLPU048E August 2016 – July 2024
The following error codes indicate a failure was detected. If the test fails, both errors will be received on a single execution of the test. One error is informational to specify the actual number of columns that failed.
ERROR CODE | DESCRIPTION |
---|---|
220 | DMD Memory BIST columns failed. The information bits of this error indicate the number of columns that failed. |
221 | DMD Memory BIST failed. |