DLPU048E August 2016 – July 2024
Table 8-1 summarizes the main application commands and indicates the operating modes in which they are available. Embedded software will flag an error if a command is used outside of the proper operating mode.
Mode key:
Read commands always return the last values that were written, or the values stored in flash if no values have been written since startup. Because of data holds, this value may be different than what is actually being displayed. For example if a new flip value is written to Display Image Orientation, but no source change has been commanded, then the value that is read back will not match what is currently being applied. The Current Source Information and Current Display Information commands allow the host to read back the settings that are currently applied to the displayed image.
COMMAND | TYPE | OP CODE | STANDBY | DISPLAY | CALIBRATION
(Not applicable for headlight) |
SECTION |
---|---|---|---|---|---|---|
System Reset | Write | 00h | Yes | Yes | Yes | Section 8.2.1 |
Read Pre-fetch | Write | 01h | Yes | Yes | Yes | Section 8.2.2 |
Read Activate | Read | 02h | Yes | Yes | Yes | Section 8.2.3 |
Operating Mode | Write | 03h | Yes | Yes | Yes | Section 8.2.4 |
Operating Mode | Read | 04h | Yes | Yes | Yes | Section 8.2.5 |
Source Select | Write | 05h | Hold Mode | Yes | Yes | Section 8.2.6 |
Source Select | Read | 06h | Yes | Yes | Yes | Section 8.2.7 |
Prepare for Source Change | Write | 07h | No | Yes | Yes | Section 8.2.8 |
Display Image Orientation | Write | 18h | Hold Mode | Hold Source | Hold Source | Section 8.2.9 |
Display Image Orientation | Read | 19h | Yes | Yes | Yes | Section 8.2.10 |
System Mode Select | Write | 1Ch | Hold Mode | Hold Source | Hold Source | Section 8.2.11 |
System Mode Select | Read | 1Dh | Yes | Yes | Yes | Section 8.2.12 |
Execute Batch Command Set | Write | 21h | Yes | Yes | Yes | Section 8.2.13 |
GPIO Configure | Write | 23h | Yes | Yes | Yes | Section 8.2.15 |
GPIO Configure | Read | 24h | Yes | Yes | Yes | Section 8.2.16 |
GPIO Outputs | Write | 25h | Yes | Yes | Yes | Section 8.2.17 |
GPIO Outputs | Read | 26h | Yes | Yes | Yes | Section 8.2.18 |
GPIO Reserved | Read | 27h | Yes | Yes | Yes | Section 8.2.19 |
Execute Non-Periodic BIST | Write | 28h | Yes | No | No | Section 8.2.20 |
External Video Checksum Control |
Write | 29h | Hold Mode | Yes | Yes | Section 8.2.21 |
External Video Checksum Control |
Read | 2Ah | Yes | Yes | Yes | Section 8.2.22 |
External Video Checksum Settings |
Write | 2Bh | Hold Mode | Yes | Yes | Section 8.2.23 |
External Video Checksum Settings |
Read | 2Ch | Yes | Yes | Yes | Section 8.2.24 |
DMD Socket Connectivity Test | Write | 2Dh | Yes | No | No | Section 8.2.25 |
DMD Socket Connectivity Test | Read | 2Eh | Yes | No | No | Section 8.2.25 |
Average Picture Level Control | Write | 2Fh | Hold Mode | Yes | Yes | Section 8.2.27 |
Loss of /Ping Control | Write | 33h | Hold Mode Yes |
Yes | Yes | Section 8.2.29 |
PWM Temperature Management Enable | Write | 35h | Yes | Yes | Yes | Section 8.2.31 |
PWM Temperature Management Enable | Read | 36h | Yes | Yes | Yes | Section 8.2.32 |
PWM Temperature Management Source | Write | 37h | Yes | Yes | Yes | Section 8.2.33 |
PWM Temperature Management Source | Read | 38h | Yes | Yes | Yes | Section 8.2.34 |
PWM Temperature Management Duty Cycle | Read | 39h | Yes | Yes | Yes | Section 8.2.35 |
Headlight Ping | Write | 46h | Yes | Yes | Yes | Section 8.2.36 |
PWM Control | Write | 47h | Yes | Yes | Yes | Section 8.2.37 |
PWM Control | Read | 48h | Yes | Yes | Yes | Section 8.2.38 |
Illumination Transition Rate | Write | 49h | Hold Mode | Yes | Yes | Section 8.2.39 |
Contrast | Read | 53h | Yes | Yes | Yes | |
De-gamma Select | Write | 54h | Hold Mode | Yes | Yes | Section 8.2.41 |
Compensation Temp Host Override | Read | 5Bh | Yes | Yes | Yes | |
Unused | 5F - 62h | |||||
ADC Single Measurement | Read | 63h | Yes | No | No | Section 8.2.44 |
Illumination Bin Select | Write | 70h | Hold Mode | Yes | Yes | Section 8.2.45 |
TPS99000-Q1 RGB Blanking Levels |
Read | 85h | Yes | Yes | Yes | |
TPS99000-Q1 TIA1 Trims | Write | 86h | No | Yes | Yes | Section 8.2.47 |
TPS99000-Q1 TIA1 Trims | Read | 87h | Yes | Yes | Yes | Section 8.2.48 |
TPS99000-Q1 TIA1 Gain | Write | 88h | No | Yes | Yes | Section 8.2.49 |
TPS99000-Q1 TIA1 Gain | Read | 89h | Yes | Yes | Yes | Section 8.2.50 |
TPS99000-Q1 TIA1 Capacitance | Write | 8Ah | No | Yes | Yes | Section 8.2.51 |
TPS99000-Q1 TIA1 Capacitance | Read | 8Bh | Yes | Yes | Yes | Section 8.2.52 |
TPS99000-Q1 TIA1 Dark Offsets | Write | 8Ch | No | Yes | Yes | Section 8.2.53 |
TPS99000-Q1 TIA1 Dark Offsets | Read | 8Dh | Yes | Yes | Yes | Section 8.2.54 |
TPS99000-Q1 TIA1 Input Offsets | Write | 8Eh | No | Yes | Yes | Section 8.2.55 |
TPS99000-Q1 DM Pulse Widths |
Read | 91h | Yes | Yes | Yes | |
TPS99000-Q1 Drive Mode | Write | 92h | No | Yes | Yes | |
TPS99000-Q1 Drive Mode | Read | 93h | Yes | Yes | Yes | Section 8.2.57 |
TPS99000-Q1 ADC Configuration | Write | 94h | No | Yes | Yes | Section 8.2.58 |
TPS99000-Q1 ADC Configuration | Read | 95h | Yes | Yes | Yes | Section 8.2.59 |
TPS99000-Q1 Illumination Sync Control | Write | 96h | No | Yes | Yes | Section 8.2.60 |
TPS99000-Q1 Illumination Sync Control | Read | 97h | Yes | Yes | Yes | Section 8.2.61 |
TPS99000-Q1 TIA2 Control | Write | 98h | Yes | Yes | Yes | Section 8.2.62 |
TPS99000-Q1 TIA2 Control | Read | 99h | Yes | Yes | Yes | Section 8.2.63 |
LED Drive Errors | Read | 9Ah | No | Yes | Yes | Section 8.2.64 |
LED Drive Errors Clear | Write | 9Bh | No | Yes | Yes | Section 8.2.65 |
TPS99000-Q1 Test Mux Select | Write | 9Ch | Yes | Yes | Yes | Section 8.2.66 |
TPS99000-Q1 TIA1 Offsets | Read | 9Fh | Yes | Yes | Yes | |
Flash Data Type Select | Write | A0h | Yes | No | No | Section 8.2.68 |
Flash Erase Data | Write | A1h | Yes | No | No | Section 8.2.69 |
Flash Write Data | Write (Bulk) | A2h | Yes | No | No | Section 8.2.70 |
Flash Read Data | Read | A3h | Yes | Yes | Yes | Section 8.2.71 |
Flash Verify Data | Read | A4h | Yes | No | No | Section 8.2.72 |
Flash Block Count | Read | A5h | Yes | Yes | Yes | Section 8.2.73 |
Flash Block CRCs | Read | A6h | Yes | Yes | Yes | Section 8.2.74 |
Unused | AA - AFh | |||||
System Software Version | Read | B0h | Yes | Yes | Yes | Section 8.2.77 |
Flash Device ID | Read | B1h | Yes | Yes | Yes | Section 8.2.78 |
DLPC230-Q1 Device ID | Read | B2h | Yes | Yes | Yes | Section 8.2.79 |
DMD Device ID | Read | B3h | Yes | Yes | Yes | Section 8.2.80 |
TPS99000-Q1 Device ID | Read | B4h | Yes | Yes | Yes | Section 8.2.81 |
System Temperatures | Read | B5h | Yes | Yes | Yes | Section 8.2.82 |
System Information | Read | BAh | Yes | Yes | Yes | Section 8.2.85 |
Unused | BC - BFh | |||||
Short Status | Read | C0h | Yes | Yes | Yes | Section 8.2.87 |
Error History | Read | C1h | Yes | Yes | Yes | Section 8.2.88 |
Clear Short Status Errors | Write | C2h | Yes | Yes | Yes | Section 8.2.89 |
Unused | F4 - FFh |