DLPU048E August 2016 – July 2024
The following error codes indicate a failure was detected:
ERROR CODE | DESCRIPTION |
---|---|
665 | External source measured active lines per frame does not match source definition. |
666 | External source measured active pixels per line does not match source definition. |
671 | External source Open LDI port pixel clock frequency is not within the allowable range. |
674 | External source parallel port pixel clock frequency is not within the allowable range. |
676 | External source pixel clock above the allowable range. |
677 | External source pixel clock below the allowable range. |
678 | External source VSYNC frequency greater than defined maximum. |
679 | External source VSYNC frequency less than defined minimum. |
913 | External source has been lost. |
914 | External source has been lost and attempt to transition to alternate source failed. |
946 | Expected VSYNC signal did not arrive in the time allocated. |