DLPU048E August 2016 – July 2024
The DLPC230-Q1 embedded software consists of two applications: the boot application and the main application. The main application includes several states, or modes, which determine the system's allowable commands and functionality at any point during operation. Typically, the Operating Mode Select command is used to transition between modes, but there are additional system conditions that can automatically trigger a mode transition. The modes and their interactions are described in the following sections.
The state diagram in Figure 4-1 provides an overview of the DLPC230-Q1 power-up procedure and the various software state transitions.
The following table summarizes general feature availability per software application and operating mode. This is not a full feature list and exceptions may exist. This is provided as an initial reference of the general purpose of each mode. The command availability tables in Chapter 7 and Chapter 8 provide more detail on the modes in which commands are available.
Boot Application | Main Application - Standby | Main Application - Display | |
Short Status / Error History | Yes | Yes | Yes |
Full Flash Program | Yes | Yes | No |
Partial Flash Program | No | Yes | No |
Non-Periodic BISTs | No | Yes | No |
Source Display | No | No | Yes |
Periodic BISTs | No | No | Yes |