DLPU057A March 2018 – April 2022
The following sections define the list of commands and their description, as supported by the Piccolo Bootloader SPI interface.
Note: The command specification is subject to correction or change as required.
Write/Read | Commands | 7-bit Address (Command ID) | Write Permissions | Section |
Reserved | 00h - 31h | |||
Read | Bootloader SW Version | 32h | Read-Only | 3.1 |
Read | Bootloader SW Status | 33h | Read-Only | 3.2 |
Reserved | 34h-70h | |||
Write/Read | Piccolo Flash Read | 71h | Always | 3.3 |
Reserved | 72h – 79h | |||
Read | Toggle Mode | 7Ah | Always | 3.4 |
Write/Read | Piccolo Program Software | 7Bh | Always | 0 |
Reserved | 7Ch | |||
<Reserved - Should not be used> | 7Dh | |||
Read | Piccolo Program Mode | 7Eh | Read-Only | 3.6 |
<Reserved - Should not be used> | 7Fh |