DLPU057A March 2018 – April 2022
This command requests a read of the ASIC Flash Data. The number of bytes required is sent as input. This command is used to read the User Information from the ASIC flash. This command starts reading from the address set by the ASIC Flash Read Setup Command (Section 3.51).
Byte | Description |
1 | Command Byte (E9h) |
2 | Length (01h) |
3 | Number of bytes to read |
4 | Checksum (Sum of bytes 1 to 3) |