DLPU057A March 2018 – April 2022 DLP3030-Q1
The Binary flash read function is used to read the piccolo flash data in binary format. This is useful to read out the main application data. The function is versatile and allows the reading of any part of the flash from any address. This is done by setting the start address by using the Set Binary Read start address function and then, using binary flash read with the required number of words as argument.