DLPU057A March 2018 – April 2022
This command sets the start address and length for the data to be programmed.
For every contiguous region, set the start address and length of the region. The length is the number of 16-bit words to be programmed in that region.
Byte | Description |
1 | Command Byte (F6h) |
2 | Length (09h) |
3 | Secondary Op-code - Start Address and Length (01h) |
4 | Start Address (lsb) |
5 | Start Address |
6 | Start Address |
7 | Start Address (msb) |
8 | Region Length (lsb) |
9 | Region Length |
10 | Region Length |
11 | Region Length (msb) |
12 | Checksum (Sum of bytes 1 to 11) |