DLPU057A March 2018 – April 2022
This command is used to set the strength and quantization step of the low pass temperature filter.
Byte | Description |
1 | Command Byte (C0h) |
2 | Length (08h) |
3 | Low Pass Filter Strength (lsb) |
4 | Low Pass Filter Strength |
5 | Low Pass Filter Strength |
6 | Low Pass Filter Strength (msb) |
7 | Low Pass Filter Quantization Step (lsb) |
8 | Low Pass Filter Quantization Step |
9 | Low Pass Filter Quantization Step |
10 | Low Pass Filter Quantization Step (msb) |
11 | Checksum (Sum of bytes 1 to 10) |
For more information on the working of the low pass filter refer to the Temperature Compensation section of the Piccolo Software Programer's Guide for the DLPC120 ASIC User’s Guide (DLPU061).