DLPU057A March 2018 – April 2022
Calibration Format Version is used to identify the internal memory format changes done to the Calibration Data File. This helps ensure that the internal calibration data is interpreted by the Piccolo SW correctly. The calibration format is defined as a 4 character string (eg: 0006). Taking 0006 as the example, the command returns the Format Version as 0x36, 0x30, 0x30, 0x30 as its data bytes.
Please refer to Piccolo Software Programmer's Guide for the DLPC120 ASIC (DLPU061) for more details about Calibration Format Version.