DLPU057A March 2018 – April 2022
This command is used to set flash binary read start address. The next binary read performed will be from the start address.
Byte | Description |
1 | Command Byte (E2h) |
2 | Length (04h) |
3 | Read Start Address (lsb) |
4 | Read Start Address |
5 | Read Start Address |
6 | Read Start Address (msb) |
7 | Checksum (Sum of bytes 1 to 6) |