DLPU062B March 2018 – January 2024 DLPC3437
Table 3-139 describes the write parameters.
Parameter Bytes | Description |
---|---|
Byte 1 | Flash batch file delay (LSB) |
Byte 2 | Flash batch file delay (MSB) |
This command is used to specify an execution delay time within a flash batch file. It can only be used within a flash batch file, and is not a valid command on the I2C interfaces.
The flash batch file delay is to be specified in units of 1 ms (for example, 500 ms = 1F4h).
Typical use of this command is in the auto-init flash batch file (batch file 0), but is valid for use in any batch file (SeeWrite Execute Flash Batch File (2Dh)).