DLPU066A March   2018  – April 2022

 

  1. 1Calibration Purpose
    1. 1.1 Calibration Purpose
    2. 1.2 Goal of Calibration
  2. 2Calibration Software and Tools
    1. 2.1 Calibration Software and Tools
  3. 3Calibration Setup
    1. 3.1 Calibration Setup
  4. 4Calibration Overview and Theory
    1. 4.1 Goal of Calibration
    2. 4.2 Calibration Background
      1. 4.2.1 Calibration File Parameters
      2. 4.2.2 Coarse Adjustment Parameter Combinations
    3. 4.3 Calibration Process
      1. 4.3.1 Calibration Pre-work: Coarse Combination Determination
      2. 4.3.2 Temperature Charaterization
      3. 4.3.3 Production PGU Calibration
  5. 5Calibration Pre-work
    1. 5.1 Pre-work Overview
    2. 5.2 Coarse Combination Determination
    3. 5.3 Strategically Adjusting Coarse Combination Parameters
      1. 5.3.1 LDC Index
      2. 5.3.2 Optical Sensor Feedback Gain
      3. 5.3.3 Current Limit
    4. 5.4 Coarse Combination Strategies
  6. 6Calibration Procedure
    1. 6.1 Calibration Procedure Overview
    2. 6.2 Calibration Sweep Setup and Coarse Combinations
    3. 6.3 Temperature Characterization
    4. 6.4 Production PGU Calibration
    5. 6.5 Generating a Calibration File
  7. 7Revision History

Generating a Calibration File

  1. Once the temperature trend sweeps and per PGU sweep is complete and calibration file can be generated.
  2. The brightness margin can be used to remove a portion of the range of a coarse combination. This is done because it may be difficult to achieve the target color point at the minimum and maximum brightness of a combination
  3. The tradeoff is that you can introduce discontinuities or reduce the maximum brightness achievable if the margins are set too aggressively.
  4. Select the brightness margins you would like for each coarse combination.
    GUID-CE0300C4-5051-4FF9-9BB8-625527EAA15C-low.pngFigure 6-14 Cal File Brightness Margins
  5. Select target color point.
    GUID-731B739C-8EAF-4858-A85C-8618F5D50F71-low.pngFigure 6-15 Cal File Target Color Point
  6. If color correction factors were recorded for your calibration procedure the can be applied by selecting the "Apply Color Correction" option.
    GUID-C32DDA0E-4096-4FAF-986A-EA4351F4E769-low.pngFigure 6-16 Cal File Color Correction Factors
  7. Select and input target brightness for each temperature range. Target brightness is dependent on color point, brightness margins and use of color correction factors. Target brightness should remain constant for each PGU calibrated.
    GUID-76448F35-7C41-4166-93BA-A000B8438FF4-low.pngFigure 6-17 Included Calibration Temperature Tables
  8. Once all options have been set, press "Generate Calibration File" and a cal file will be generated.
  9. During the generation of the cal file, feedback will be provided to the user.
  10. If there are errors or warnings during the generation of the cal, the errors should be reviewed and corrective action can be taken. In most cases the cal file will still be generated but may have some discontinuities in the dimming range.
  11. In the case where a continuous dimming range cannot be achieved you may reduce the brightness margins. Often times a small discontinuity is imperceptible.
GUID-610C3B2D-B694-4010-AFB7-FCE533E94B7A-low.pngFigure 6-18 Example Calibration Table Output