DLPU081B January 2019 – January 2024 DLPC3479
Table 3-64 describes the write parameters.
Parameter Bytes | Description |
---|---|
Byte 1 | Maximum red LED current (LSByte) |
Byte 2 | Maximum red LED current (MSByte) |
Byte 3 | Maximum green LED current (LSByte) |
Byte 4 | Maximum green LED current (MSByte) |
Byte 5 | Maximum blue LED current (LSByte) |
Byte 6 | Maximum blue LED current (MSByte) |
This command sets the maximum LED currents that can be used when CAIC is enabled or disabled. When CAIC is enabled, the maximum LED currents may be further limited by the CAIC LUTs stored in the flash. The parameter specified by this command has a resolution of 10 bits. The unused most significant bits should be set to 0.