DLPU082C August 2021 – March 2024 DLPC7540
This command is used to get the gain values set by CMD_ SetBlendMapGainValues. Select the same color channel select option that was used in CMD_ SetBlendMapGainValues and pass the index and number of values to get.
If compressed values were set, then this command returns compressed values. If uncompressed values were set, this command returns uncompressed values.
Byte Index | Value | Description |
---|---|---|
0 | 0x54 | Command packet header (destination 4 ,length present, response required) |
1 | 0x2B | Command opcode |
2 | 0x00 | Broadcast selected in color channel select |
3-4 | 0x0000 | Start index = 0 |
5-6 | 0x0040 | Number of values to be read. This example reads 64 values. |