DLPU094 July 2020 DLP5530S-Q1
In creating a functional safety concept and doing the functional safety analysis, TI generates a series of assumptions on system level design, and requirements. These assumptions (sometimes called Assumptions of Use) are listed below. Additional assumptions about the detailed implementation of safety mechanisms are separately located in Section 7.3.
The DLP5530S-Q1 Functional Safety Analysis was done under the following system assumptions:
During integration activities these assumptions of use and integration guidelines described for this component shall be considered. Use caution if one of the above functional safety assumptions on this component cannot be met, as some identified gaps may be unresolvable at the system level.