DLPU101D December 2020 – July 2024 DLPC900
When deleting images from flash, the flash device is erased and then updated with the firmware that contains the new images. In the event the flash is accidentally corrupted, follow the instructions under JTAG Flash Programming (see Section 6.11) to reload the original firmware. To avoid accidental erasure or corruption of the flash device, TI recommend to operate in Pattern On-The-Fly Mode.
The user must exercise caution when selecting the correct firmware file. Make sure the firmware file is version 3.0 or later. Using version 2.0 or earlier renders the EVM inoperable. Version 6.0 or later is recommended.
Follow these steps to begin deleting images from the firmware file:
The updated firmware file has no images. TI recommends to rename the updated firmware file with a specific name so that the file can be reused as a firmware file that has no images.