DLPU101D December 2020 – July 2024 DLPC900
The DLP LightCrafter Single DLPC900 EVM is a flexible, ready-to-use evaluation module which, when coupled to one of the DLP LightCrafter DMD EVMs, enables the sending of customer created patterns from the DLPC900 Controllers to the attached DMD for display at the customer determined pattern rates. The DLP LightCrafter Single DLPC900 EVM and the DMD EVMs are offered for purchase separately so that customers can determine which elements to piece together for an application evaluation system.
The following items are not included with the EVM and need to be purchased separately if needed for customer evaluation: