DLPU101D December 2020 – July 2024 DLPC900
Creating pattern sequences with DMD Block Load achieves higher pattern rates by using a subset of the DMD blocks. See DMD Block Load command in the DLPC900 Software Programmer’s Guide (DLPU018) for a description of this command.
Follow these steps to create a Pattern On-The-Fly pattern sequence with only three DMD active blocks.
Notice that pattern 0 is displayed the same way as pattern 2 even though pattern 0 contains image data for all blocks showing that only blocks 6, 7, and 8 are active while all other blocks are in the off state.
The performance of the mirrors in the blocks that are not active are affected by prolonged use of being in the off state. Enable DMD Idle Mode as often as possible to optimize the mirrors. This mode provides a 50/50 duty cycle across the entire DMD mirror array, where the mirrors are continuously flipped between the on and off states. See DMD Idle Mode command in the DLPC900 Software Programmer’s Guide (DLPU018) for a description of this command. The DMD Idle Mode command is located in Section 6.6.7 within the Pattern Mode panel.