DLPU101D December 2020 – July 2024 DLPC900
A batch file can be added to the firmware to be used as the default batch file to be executed during the power-up sequence of the DLPC900. Or a batch file can be added to be executed at any time after the power-up sequence has completed to perform some action. Some special considerations must be taken if adding pattern images and a batch file to the firmware image. See NOTE at end of Section 6.9.1.2 for a description of these considerations. Follow these steps to add the example batch file from the previous section to the firmware.
The user must exercise caution when selecting the correct firmware file. Install DLP LightCrafter GUI version 5.x or later and select FW version 6.x or higher. Operating or updating the firmware on the DLPC900 LightCrafter GUI version 4.x (or earlier) renders the EVM inoperable. Note: The DLP5500 DMD is only supported by GUI version 5.2.x and FW version 6.2.0.
When updating the firmware for the DLPC900 Single Controller EVM, there is only one firmware image file (*.img).
If the batch file is to be a default batch file to be executed during the power-up sequence, then continue to step 12, otherwise go to step 13.
The name of the firmware file created by the GUI includes a timestamp, verifying that new firmware does not overwrite any previously created firmware files.