DLPU101D December   2020  – July 2024 DLPC900

 

  1.   1
  2.   Trademarks
  3.   Read This First
  4. About This Guide
  5. Related Documentation from Texas Instruments
  6. If You Need Assistance
  7. DLP LightCrafter Single DLPC900 EVM Overview
    1. 4.1 Welcome
    2. 4.2 DLP LightCrafter Single DLPC900 Evaluation Module (EVM) Hardware
    3. 4.3 EVM Board
    4. 4.4 Other Items Needed for Operation
    5. 4.5 DLP LightCrafter Single DLPC900 Connections
      1. 4.5.1 DLP LightCrafter Single DLPC900 LED Enable and PWM Outputs
      2. 4.5.2 DLP LightCrafter Single DLPC900 Trigger Input and Output Voltage Selectors
    6. 4.6 DLP LightCrafter Single DLPC900 EVM Flex Cable
    7. 4.7 DLP LightCrafter Single DLPC900 EVM and DMD EVM Assembly
  8. Quick Start
    1. 5.1 Power-up the DLP LightCrafter Single DLPC900 EVM
    2. 5.2 Creating a Simple Pattern Sequence
  9. Operating the DLP LightCrafter Single DLPC900 EVM
    1. 6.1  DLP LightCrafter Single DLPC900 Control Software
    2. 6.2  PC Software
    3. 6.3  System Common Controls
      1. 6.3.1 Operating Mode
      2. 6.3.2 Connected DMD Type
      3. 6.3.3 EVM Information
      4. 6.3.4 Status
    4. 6.4  System Settings
    5. 6.5  Video Mode
      1. 6.5.1 Video Support
    6. 6.6  Pattern Modes
      1. 6.6.1 Menu Bar
      2. 6.6.2 Creating a Pattern Sequence in Pattern On-The-Fly Mode
      3. 6.6.3 Creating a Pattern Sequence in Pre-Stored Pattern Mode
      4. 6.6.4 Reordering a Pattern Sequence using the Edit LUT Feature
        1. 6.6.4.1 Special Considerations for Input Triggers when using the Edit LUT Feature
      5. 6.6.5 Creating a Pattern Sequence in Video Pattern Mode
      6. 6.6.6 Creating a Pattern Sequence With DMD Block Load
      7. 6.6.7 Pattern Settings
    7. 6.7  Batch Files
      1. 6.7.1 Execute Batch File
      2. 6.7.2 Creating and Saving Batch Files
        1. 6.7.2.1 Creating and Saving a Batch File Using the GUI
        2. 6.7.2.2 Creating a Batch File Using a Text Editor
      3. 6.7.3 Loading a Batch File
      4. 6.7.4 Adding a Batch File to the Firmware
    8. 6.8  Peripherals
      1. 6.8.1 Peripherals Tab
      2. 6.8.2 Debug Tab
    9. 6.9  Firmware
      1. 6.9.1 Adding or Removing Patterns from the Firmware
        1. 6.9.1.1 Deleting Images
        2. 6.9.1.2 Adding Images
        3. 6.9.1.3 Adding Both Images and Batch Files
      2. 6.9.2 Reprogram Firmware for a Different Supported DMD
    10. 6.10 Flash Device Parameters
    11. 6.11 JTAG Flash Programming
    12. 6.12 Programming an EDID
  10. Connectors
    1. 7.1  Input Trigger Connectors
    2. 7.2  Output Trigger Connectors
    3. 7.3  DLPC900 UART
    4. 7.4  DLPC900 I2C Port 0
    5. 7.5  DLPC900 I2C Port 1
    6. 7.6  DLPC900 I2C Port 2
    7. 7.7  JTAG Boundary Scan
    8. 7.8  GPIO and PWM
    9. 7.9  Power
    10. 7.10 External Parallel Video Connector
  11. Power Supply Requirements
    1. 8.1 External Power Supply Requirements
  12. Safety
    1. 9.1 Caution Labels
  13. 10Revision History

Creating a Batch File Using a Text Editor

Use a text editor to add the same three commands in the previous example. Refer to Appendix B in the DLPC900 Programmer’s Guide for the list of command descriptors supported by the DLPC900.

When adding a command descriptor to the file, a colon must be between the descriptor and the parameters. Use a space between the colon and each parameter and use ‘0x’ for each byte in the parameter list. Remember that the parameters are least significant byte first. The lines below show what is to be in the text file.

FLIP_SHORT:0x01
CHANNEL_SWAP:0x0A
LED_CURRENT:0x64 0x64 0x64

Once all three commands are added, save the file as a text file and use a name to describe what the batch file does.