DLPU102C December 2020 – July 2024
GUI 5.3 Added debug functions shown in Figure 4-21.
Click the Debug Tab button at the side of the Peripherals Panel to display Figure 4-21.
Selecting the Enable Debug mode checkbox enables the debug functions shown in on the Debug Tab.
Select the desired controllers in the From box.
There are two virtual interfaces to assist in debugging. For example Reading from or Writing to some addresses can result in changes in other memory locations. The result of writing to a memory using Interface 1 can be tracked in Interface 2.
The following are valid memory address ranges:
Debug Masks - detailed descriptions:
Max String Length - reads the maximum allocated string size for the debug message
Currently Used - reads the string size currently used by the debug message
Select the Record result check box to record the result of running a provided batch file. Results are recorded in the same directory that the batch file resides.
Use Open memory access batch File button to navigate to a memory access batch file provided.
Use Run memory access batch file button to run the batch file selected by the Open memory access batch File.
Select the Enable or Disable button to show or hide diagnostic log windows. Enabling this option shows a command log window under the main GUI window are as shown in Figure 4-22.
These logs are available:
For the Projector Control log and Command log the following options are available: