DLPU109A May   2021  – September 2024

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1DLPC7540EVM, DLP471TEEVM, DLP472TEEVM, and DLP650TEEVM Overview
    1. 1.1 Introduction
    2. 1.2 What is in the DLP471TEEVM, DLP472TEEVM, DLP650TEEVM, and DLPC7540EVM Evaluation Modules?
    3. 1.3 EVM Boards
    4. 1.4 Other Items Needed for Operation
    5. 1.5 DLPC7540EVM, DLP471TEEVM, DLP472TEEVM, and DLP650TEEVM EVM Flex Cable
  6. 2Hardware
    1. 2.1 Additional Images
    2. 2.2 Connections
      1. 2.2.1 DLPC7540EVM Connections
      2. 2.2.2 DLP471TEEVM, DLP472TEEVM, and DLP650TEEVM Connections
        1. 2.2.2.1 Test Points
        2. 2.2.2.2 Connectors
    3. 2.3 Power Supply Requirements
      1. 2.3.1 External Power Supply Requirements
  7. 3Software
    1. 3.1 Quick Start
      1. 3.1.1 Downloading the Software
      2. 3.1.2 Connecting the DLP471TEEVM, DLP472TEEVM, or DLP650TEEVM, to the DLPC7540EVM
      3. 3.1.3 Powering-up the DLPC7540EVM and Preparing to Program the DLPC7540EVM
      4. 3.1.4 Programming the DLPC7540EVM and Displaying a SPLASH Image
      5. 3.1.5 Troubleshooting
  8. 4Hardware Design Files
  9. 5Additional Information
    1. 5.1 Safety
      1. 5.1.1 Caution Labels
      2. 5.1.2 If You Need Assistance
    2. 5.2 Trademarks
  10. 6Related Documentation
  11. 7Revision History

Programming the DLPC7540EVM and Displaying a SPLASH Image

Follow these steps to download and configure the DLPDLC-GUI for DLPC7540 operation:

  1. Download the DLPDLC-GUI and the Firmware SW package that includes the Firmware binary (.img) files for DLP471TE, DLP472TE, and DLP650TE.
  2. Install and open the DLPDLC-GUI
  3. Setting up communication preferences:
    1. DLPDLC-GUI supports USB and I2C communication. To change these settings in GUI, please go to Debug screen and select Connection tab.
    2. For USB, select the USB interface and click Connect; see Figure 3-3.
      Note: USB is the preferred interface to download the firmware flash image to the EVM as USB is much faster than I2C and does not require any additional hardware.
      DLPC7540EVM Command
                                    Interface Settings Figure 3-3 Command Interface Settings
    3. Verify that EVM Status shown at bottom left of GUI says Connected, Bootloader Mode indicating you are ready to load image file into EVM.
  4. Flash Loader Configuration:
    1. Go to Firmware screen, select Update Firmware tab. Click on the folder icon to browse for the applicable firmware depending on the actual DMD that is connected to DLPC7540EVM. Once firmware image file is selected, click on Start Update; see Figure 3-4.
    2. Wait for the programming progress to indicate that firmware update is complete.
    3. Turn off the EVM by toggling the SW1 and SW5 switches in that order to off position. Remove the jumper from J9 and install back to J67.
    4. Turn on the EVM by toggling the SW5 and SW1 switches in that order to on position. After about 3 seconds, users see D5, D6, and D7 LEDs steadily on and D15 LED flashing. The DLP Texas Instruments logo is visible on the DMD; see Figure 3-5.
      DLPC7540EVM Loading the
                                    Flash Image Figure 3-4 Loading the Flash Image
      Note:

      If there is an issue with USB communication, then turn off DLPC7540EVM and disconnect then reconnect USB cable and power on board.

      DLPC7540EVM Splash Image
                                    Displayed on DMD Figure 3-5 Splash Image Displayed on DMD