DLPU114 August 2024 DLPC8445
In the case that video data is suddenly disconnected or halted, the controller will continue transmitting the last valid data that is has received. This may result in image artifacts. It is recommended to monitor the video source via a host processor controlling the video front-end or the VBO status (see Section 9.4.11) in the case of a V-by-One front end to ensure the state of the video source. If this video source is found to be lost it is recommended to switch the source to an image curtain, test pattern, or splash screen.