In order to properly set up HDR, the following steps should be performed:
- Ensure that HDR is enabled for the Look being used.
- HDR is typically enabled by Looks by default.
- Set the System Brightness Range Setting (Section 9.2.5). Typical values are
between 0.1 and 400 nits.
- Set HDR Source Configuration (Section 9.2.1)
- Set HDR Strength (Section 9.2.3)