DLPU114 August 2024 DLPC8445
This command is used to read data from flash. This command shall be called only after setting the start address and size using the Initialize Flash Read Write command. Flash Read commands can be chained until the initialized number of bytes are returned. The BootROM will auto-increment the address and size for each command. Only the initialized number of bytes will be returned. Calling the function after returning requested data will result in command failure. This command supports variable sized response. Number of bytes to write is always expected to be a multiple of 4 bytes. Command returns error if it is not multiple of 4.