DLPU114 August 2024 DLPC8445
This command sets HDR strength which adjusts the electro-optical transfer function that is applied on the input HDR video signal. HDR strength can vary with the ambient brightness level. HDR strength is not applicable for HLG transfer function set by HDR source configuration. Changing the HDR strength for HLG only affects half of the EOTF processing, leading to unpredictable results.
Please note that this command will be deprecated in future releases.