DLPU114 August 2024 DLPC8445
This command reads the LED duty cycles after adjustments by the WPC algorithm have been made.
When WPC is enabled via command Set WPC Enable, WPC automatically adjusts the LED duty cycles until the target white point is achieved. A light sensor embedded in the system is used to monitor the illumination light applied to the DMD.
Before reading duty cycles with this command, make sure WPC is enabled.
The target white point, and the target duty cycles that nominally achieve this white point, can be read with command Get Look. To maintain the target white point the actual LED duty cycles used by WPC will vary from the target values as needed to compensate for system opto-mechanical tolerances and LED performance drift with temperature and aging.