DLPU114 August 2024 DLPC8445
This command enables the WPC function.
White Point Correction (WPC) is a function that automatically adjusts the duty cycles for the red, green, and blue LEDs until the target white point is achieved. The target white point for each Look is set in the firmware. Use command Get Look to read the target white point for the active Look.
When enabled, WPC runs continuously. The controller regularly reads measured data from the light sensor and makes updates to the duty cycles. Continuous operation assures that any drift in the white point over time such as due to LED heating is removed and the target white point is always maintained.
For proper convergence and operation of the WPC algorithm, WPC Sensor Calibration Data must be loaded via Set WPC Calibration Data command or via EEPROM before enabling WPC.
Note that the Dynamic Black commands will take precedence over other color processing algorithms.