DLPU114 August 2024 DLPC8445
This command specifies the cropping applied to input images.
This command applies to all sources including test patterns, splash screens, and external sources.
Cropping is done prior to the scaling function in the controller. As such, the size difference between the cropped image size and displayed image size determines the amount of scaling needed in both dimensions if scaling using WRP is enabled.
This command must be followed with a Write Execute Display command to be applied.
The cropping rules are demonstrated in the following figure.