DLPU114 August 2024 DLPC8445
This command initiates the execution of queued display commands.
Due to an extended setup and reconfiguration time, some display commands have been made into queued commands. This means that the commands will not be executed until the Execute Display Command is called. Grouping multiple queued commands allows for a reduced configuration time.
The queued commands include but are not limited to:
1. Set Input Image Size Queued
2. Set Image Crop Queued
3. Set Display Size Queued
4. Set Pre-Defined Timings Queued
5. Any XPR control commands
6. Set VBO Configuration
7. Write Splash Screen Select
It is recommended to follow this command with Read Execute Display Status to confirm that this has been executed without error.