DLPU114 August 2024 DLPC8445
This command sets the drive levels for each LED. The drive levels are set only if the LED Channel is valid.
The currents for each individual LED can be controlled independently. The limits for the current level set is decided by the minimum and maximum values specified for the system in the flash image. The command will not return an error if the current is outside the expected range. Instead, it will automatically limits to minimum limit if the value is less then the minimum limit and limits to maximum limit if the value is greater then the maximum limit. Reading back the values will guarantee whether it is applied directly or limited against the minimum and maximum. The applicable LED must be enabled for the effect to be seen on the display.
When the color processing algorithms (WPC and Dynamic Black) are disabled, this command directly sets the LED currents (the R, G, and B 10-bit values provided are sent directly to the DLPA PMIC by the controller via SPI). If color processing algorithm is enabled, then this command will not take effect immediately.
When an all-white image is displayed and color processing algorithms are disabled, this command allows the system white point to be adjusted while at the same time establishing the total LED power for the display module.