DLPU114 August 2024 DLPC8445
This command sets number of pixels that can be clipped by Dynamic Black Algorithm. Number of clip pixels should not be more than 4% of total pixels. A typical value should be less than or equal to 1.5% of the total number of pixels with respect to the display size. This command should only be exercised during the development phase with DB and clip pixels being set in the firmware.