DLPU114 August 2024 DLPC8445
This command is applicable only if TMP411A temperature sensor is installed in the system. If properly configured, the thermistor should not return a negative value.
A local reading means that the reading is directly at the TMP411. A remote reading would mean that the reading is taking place at te test point pins of the DMD (indirectly at the DMD).