DLPU114 August 2024 DLPC8445
This command sets the current data update lock state for EEPROM/FLASH.
When lock is set, all writes to EEPROM/Flash settings and/or calibration data from application software will not be actually written to the EEPROM/Flash. The locked mode is to be used only in factory where user wants to play around with various settings without actually recording them in the EEPROM/Flash. In Normal Use mode, the lock is not supposed to be set.