DLPU114 August 2024 DLPC8445
When this flag is set, the default factory settings are applied on next power-up without invalidating (erasing) the settings stored in the EEPROM/Flash. Upon power up, change in any setting will not be updated to the EEPROM/Flash irrespective of commit mode. If Data Storage mode is EEPROM and commit mode is immediate, setting this flag will restart the system immediately. If data storage is Flash, the Commit Data command needs to be given and system will not start restart immediately.