DLPU114 August 2024 DLPC8445
This command is used to switch between the commit modes - immediate and update via command, during run-time. This command is only applicable if data storage mode is EEPROM. In Immediate mode data will be stored in EEPROM as it is updated. In Command mode updated data will be only stored once the Commit Data command is given.