DLPU114 August 2024 DLPC8445
This command changes the Look of the displayed image by attempting a Write Look Select value by the user which will trigger to sequence selection. The value should be within the looks specified in the firmware image.
It is recommended to add a delay of approximately 50ms after this command if it is to be followed by a Color Duty Cycle command.