DLPU114 August 2024 DLPC8445
Get System Status | |
---|---|
Return Parameter(s) | |
Byte | Description |
Byte 0 |
System Status bit0: System Init Done bit indicates, system bring up is complete and HOST_IRQ pin is pulled high. bit1: The System Error bit indicates an error for the system (controller chipset or peripheral hardware controlled by the chipset such as LEDs).Details about system errors are available using the Get System Errors command. bit2: The Video Port Error bit indicates invalid input timing on the active video port.Details about video port errors are available using the Source Timing and Errors command. |
Byte 1 |
System Mode bit0: The Actuator Calibration Mode bit indicates that system is currently in actuator calibration mode.Multiple system functionalities will be bypassed in this mode. |
Byte 2 |
Sequencer and LED Status bit0: Sequencer phase lock bit indicates Sequencer Phase is locked with incoming video source Vsync.Phase lock will not happen in case of Splash input or asynchronous input source. bit1: Sequencer frequency lock bit indicates Sequencer Frequency is locked with incoming video source Vsync.Frequency lock will not happen in case of Splash input or asynchronous input source. bit2: Red Enabled bit3: Green Enabled bit4: Blue Enabled |