DLPU114 August 2024 DLPC8445
The controller contains an Arm® Cortex R4F processor along with additional functional blocks for image processing and chipset control. TI provides software as firmware to be stored in an SPI flash memory connected to the controller. The firmware consists of the MainApp code (used by the Arm processor) along with other configuration and operational data required by the system for normal operation. The controller and its accompanying DLP chipset components require this proprietary software to operate.
The firmware must be programmed into the SPI flash memory. The DLPC8445 downloads the main application from Flash into the Arm processor instruction RAM at power-up and also periodically accesses the operational data in Flash during runtime. The available controller functions depend on the firmware version in Flash. Different firmware is required for different chipset combinations (such as when using different DMD or PMIC devices). Visit the applicable controller's product folder on ti.com and go to the DLP Pico Firmware Selector, or contact TI for the latest firmware.