DLPU114A August 2024 – November 2024 DLPC8445
In order for three dimensional images to be perceived, the controller projects differing left and right frames sequentially. A complete 3D frame will have a left and a right subframe which will be shown or blocked via 3D glasses. As a result the controller will be transmitting frames as 120Hz for a 60Hz frame to be perceived. For proper use, an external trigger signal must drive into the GPIO that acts as the left/right frame sync trigger, known as the 3DLR trigger. In the case of the DLPC8445, this input is GPIO_21.
A proper setup for 3D video transmission would be the following: