DLPU114A August 2024 – November 2024 DLPC8445
When using the I2C protocol, the target component pulls the clock line low when it needs to indicate it is busy processing and cannot accept any more data from the host. Be aware that when there are multiple target devices on the same bus, the entire communication on the bus gets halted until the busy peripheral component releases the bus. To prevent this undesirable effect, the controller supports the following options for the host: